2024-04-17 1:57 AM
Hi,
I´m just starting with Matter over Thread (with the Lighting-App from github).
I´m a little bit confused which binary is for which purpose, because the file various file names:
- BLE_Thread_dynamic / static (from STM32Cube_FW_WB_V1.19.0)
- Thread_xxx (from STM32Cube_FW_WB_V1.19.0)
- BLE_Thread_ForMatter (from the github example)
Especially for me the difference between Thead and Thread for Matter is not clear.
Which is the right one for the Github Lighting example?
Best regards,
Achim
2024-04-24 9:51 AM
Hello,
To work with Matter over Thread, you should use the X-CUBE-MATTER available on ST website. To have more details on each binary you can refer to the release notes, for Matter you should use the binary available in the X-CUBE-MATTER:
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.