2020-06-30 4:00 PM
RE: STM32Cube_FW_WB_V1.7.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRateFreeRTOS\Core\Src\stm32_lpm_if.c
/**
* The switch on HSI before entering Stop Mode is required on Cut2.0
* It is useless from Cut2.1
*/
Switch_On_HSI( );
Seems like it would be great for efficiency if we could deterministically avoid this work in and out of power off mode.
Solved! Go to Solution.
2020-07-01 5:45 AM
Note that all these remarks aound CUT2.0 are removed from the next CubeWB FW package.
2020-07-01 3:26 AM
As far as I know, CUT2.0 never went in mass production.
Only CUT2.1 is used on Nucleo board.
This comment is there for the very first development versions of the STM32WB.
2020-07-01 5:43 AM
When did you buy this nucleo board?
2020-07-01 5:45 AM
Note that all these remarks aound CUT2.0 are removed from the next CubeWB FW package.
2020-07-01 10:42 AM
Thanks, @Remi QUINTIN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.