2020-07-01 1:50 AM
In my STM32CubeIDE version 1.3.1 Build: 6291_20200406_0752 (UTC), the IDE automatically added the "--specs=nano.specs" for the GCC assembler.
However, the GCC assembler doesn't recognized the "--specs=nano.specs" option.
I want to remove or disable the "--specs=nano.specs" for the GCC assembler as.
My STM32 mcu is ARM cortex-m4 STM32WB55.
My EVB is STM32WB55 Nucleo Pack.
The GCC assembler version is GNU assembler version 2.30.0 (arm-none-eabi) using BFD version (GNU Tools for STM32 7-2018-q2-update.20190328-1800) 2.30.0.20180329
The build error message is as following.
make all
arm-none-eabi-as -mcpu=cortex-m4 -mthumb -g -c --specs=nano.specs -mfloat-abi=soft -mthumb -o "MDK-ARM/startup_stm32wb55xx_cm4.o" "../MDK-ARM/startup_stm32wb55xx_cm4.s"
arm-none-eabi-as: unrecognized option `--specs=nano.specs'
make: *** [MDK-ARM/subdir.mk:15: MDK-ARM/startup_stm32wb55xx_cm4.o] Error 1
"make all" terminated with exit code 2. Build might be incomplete.
Thanks.
Karl
2020-07-01 2:07 AM
How did you end up with CubeIDE calling arm-none-eabi-as instead of arm-none-eabi-gcc? AFAIK it should invoke
arm-none-eabi-gcc -x assembler-with-cppinstead, which would recognize but ignore --specs.
Anyway, if it has to remain that way with arm-none-eabi-as, try to switch off --specs=nano.specs in the MCU Settings dialog, and add it back under Linker / Miscellaneous / Other flags.
2020-07-02 2:01 AM
Hi Berendi,
Thanks. I will try the "arm-none-eabi-gcc " as assembler.
I compose a GNU Makefile to build STM32Cube_FW_WB_V1.7.0\...\BLE_HeartRateFreeRTOS application. It built OK but it cannot bootup normally.
I import the Makefile and BLE_HeartRateFreeRTOS into STM32CubeIDE version 1.3.1 for debugging. Then the STM32CubeIDE got some java Null string errors in MCU Settings dialog.
I am trying to fix these error.
Karl
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.