2025-02-25 7:51 AM - last edited on 2025-02-26 5:40 AM by Amel NASRI
Hello,
I have developed a LoRa application based on the LoRaWAN EndNode example, with some custom code and using the .ioc configuration. I am working on the Nucleo board STM32WL55JC1.
Now, I would like to migrate my application to the LoRa End Node FUOTA example while keeping my existing development. However, I am unsure about the best approach to achieve this.
Should I replace the LoRa End Node project inside the FUOTA example (though I assume I will miss some FUOTA-specific classes and functions)?
Or should I integrate the additional FUOTA-related projects (KMS_blob, EWARM,BFU, SECoreBin,Linker ...) around my existing LoRa application?
Any guidance or best practices would be greatly appreciated.
Thanks!
2025-03-24 8:13 AM
Hello @SamyHaouaraUTC
What I suggest you is to try the same implementation as on the example LoRaWAN_FUOTA available under STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.