2025-07-10 5:13 PM
I am using the NUCLEO-WL33CC1 (for 868 MHz freq) and I tried the LPAWUR feature based on the Github examples that you provided:
https://github.com/STMicroelectronics/STM32CubeWL3/tree/main/Projects/NUCLEO-WL33CC/Demonstrations/LPAWUR/LPAWUR_WakeupRadio_Rx
The issue is that the range that I get is a max of 3 meters, no more that this. I already soldered the C3 capacitor, that is by default missing, with a value of 100pF. The L3 is 5.6nH and L4 is 6.8nH based on the schematics (MB2029) of the NUCLEO witch matches the values that are in the User Manual of the Nucleo (UM3418).
Questions:
MRSUBG_RadioInitStruct.outputPower = 14;
MRSUBG_RadioInitStruct.PADrvMode = PA_DRV_TX_HP; LPAWUR_RadioInitStruct.AgcMode = AGC_MODE_OFF;
2026-04-29 11:21 AM
I appear to be having the same issue. Did you ever get around to figuring this out.
I did set the AGC mode to ON, for LPAWUR, and the output power to 20 with PA_DRV_TX_TX_HP, and still no luck.
2026-04-30 5:44 AM
Hi Marko26,
use the STM32Cube_FW_WL3_V1.4.0\Projects\NUCLEO-WL33CC\Demonstrations\MRSUBG\MRSUBG_WakeupRadio_Tx project for the transmitter, and set 20 dBm as output power and PA_DRV_TX_TX_HP as PA drive mode.
use the STM32Cube_FW_WL3_V1.4.0\Projects\NUCLEO-WL33CC\Demonstrations\Command_Line_Interface\CLI project for the receiver, so you can use the STM32CubeWiSE-RadioExplorer (I suggest latest version, v1.3.1)
In the RadioExplorer, connect the RX board and click the Config button in the System settings, Radio settings, Data coding, Packet settings and Wakeup Radio settings menu. Then, go to Wakeup RX packet test and click Start.
For more information on how to use the RadioExplorer, here is the documentation: https://www.st.com/resource/en/user_manual/um3400-stm32cubewiseradioexplorer-software-description-stmicroelectronics.pdf
Push the B2 button on the TX board and you will see the incoming packets in the RadioExplorer.
The range of the LPAWUR is at least 10 meters in line of sight.
The AGC is not involved in this scenario, it works at high power to reduce the incoming power.
BR,
Filippo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.