2024-11-01 10:51 AM
Hello,
It seems that the example BLE_p2pServer_ota works with an operating system? I want to forward certain payload data to a UART2 interface via DMA after a connection has been established.
Where is the right place to insert a HAL_UART_Tx_DMA transmission function in the code?
In the example provided, the function to check the payload is queried in the p2p_server_app.c file in line 122:
if(p_Notification->DataTransfered.p_Payload[1] == 0x01)
{
BSP_LED_On(LED_BLUE);
LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 ON\n");
P2P_SERVER_APP_Context.LedControl.Led1 = 0x01; /* LED1 ON */
// Here, i want to include the HAL_USART_Tx function ...
}
if(p_Notification->DataTransfered.p_Payload[1] == 0x00)
{
BSP_LED_Off(LED_BLUE);
LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 OFF\n");
P2P_SERVER_APP_Context.LedControl.Led1 = 0x00; /* LED1 OFF */
}
For example, here i want to transfer the string "LED ON" to USART2.
Is this the right place to insert the code?
Solved! Go to Solution.
2024-11-20 1:18 AM
Hello @ledi001
Yes, you can add the function of send data throw USART2 on the line you mentioned.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-20 1:18 AM
Hello @ledi001
Yes, you can add the function of send data throw USART2 on the line you mentioned.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.