2024-12-03 3:19 AM - last edited on 2024-12-03 3:24 AM by Andrew Neil
Hi,
I am using the example ble_p2pServer_ota with STm32WBA55. I would send a packet between a client and a server with more than 20 bytes.
Here is part of the code from p2p_server.c:
When i debug the code, the value of Attr_Data_Length is correct until i send up to 20 bytes. If i want to send 25 bytes, the value of Attr_Data_Length remains at 20.
case ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE:
{
/* USER CODE BEGIN EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_BEGIN */
/* USER CODE END EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_BEGIN */
p_attribute_modified = (aci_gatt_attribute_modified_event_rp0*)p_blecore_evt->data;
notification.ConnectionHandle = p_attribute_modified->Connection_Handle;
notification.AttributeHandle = p_attribute_modified->Attr_Handle;
notification.DataTransfered.Length = p_attribute_modified->Attr_Data_Length;
notification.DataTransfered.p_Payload = p_attribute_modified->Attr_Data;
Then i cheched the value of ATT_MTU size in file app_config.h. This value is 251 which is correct.
#define CFG_BLE_ATT_MTU_MAX (251)
Then i changed the default ATT_MTU size (minimum MTU value that GATT must support) from 23 to 50 in file ble_bufsize.h.
#define BLE_DEFAULT_ATT_MTU 50 //23
But nothing has changed. Can anyone help?
2024-12-25 8:00 AM
Hello @ledi7
To be able to send more then 20 bytes, you have to follow the Extended advertising feature. For more details, you may take a look at this Wiki. Also, the examples BLE_p2pClient_Ext and BLE_p2pServer_Ext may can help you to understand how to do that.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.