2024-02-21 3:19 AM
Hello, I am working with STM32WBA52 and I am using the X-Nucleo-NFC07A1 Tag to try to perform BLE OOB Pairing. From the sparse existent documentation regarding this subject, I have understood that the SecurityParams_t structure had a flag to indicate OOB Pairing support, however this flag does not exist anymore.
typedef struct
{
/* IO capability of the device */
uint8_t ioCapability;
/**
* Authentication requirement of the device
* Man In the Middle protection required?
*/
uint8_t mitm_mode;
/* Bonding mode of the device */
uint8_t bonding_mode;
/**
* this variable indicates whether to use a fixed pin
* during the pairing process or a passkey has to be
* requested to the application during the pairing process
* 0 implies use fixed pin and 1 implies request for passkey
*/
uint8_t Use_Fixed_Pin;
/* Minimum encryption key size requirement */
uint8_t encryptionKeySizeMin;
/* Maximum encryption key size requirement */
uint8_t encryptionKeySizeMax;
/**
* fixed pin to be used in the pairing process if
* Use_Fixed_Pin is set to 1
*/
uint32_t Fixed_Pin;
/**
* this flag indicates whether the host has to initiate
* the security, wait for pairing or does not have any security
* requirements.
* 0x00 : no security required
* 0x01 : host should initiate security by sending the slave security
* request command
* 0x02 : host need not send the clave security request but it
* has to wait for paiirng to complete before doing any other
* processing
*/
uint8_t initiateSecurity;
/* USER CODE BEGIN tSecurityParams*/
/* USER CODE END tSecurityParams */
}SecurityParams_t;
-> First I configure the authentication parameters:
/* Initialize authentication */
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.mitm_mode = CFG_MITM_PROTECTION;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMin = CFG_ENCRYPTION_KEY_SIZE_MIN;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMax = CFG_ENCRYPTION_KEY_SIZE_MAX;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.Use_Fixed_Pin = CFG_USED_FIXED_PIN;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.Fixed_Pin = CFG_FIXED_PIN;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.bonding_mode = CFG_BONDING_MODE;
/* USER CODE BEGIN Ble_Hci_Gap_Gatt_Init_1*/
/* USER CODE END Ble_Hci_Gap_Gatt_Init_1*/
ret = aci_gap_set_authentication_requirement(bleAppContext.BleApplicationContext_legacy.bleSecurityParam.bonding_mode,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.mitm_mode,
CFG_SC_SUPPORT,
CFG_KEYPRESS_NOTIFICATION_SUPPORT,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMin,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMax,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.Use_Fixed_Pin,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.Fixed_Pin,
CFG_BD_ADDRESS_TYPE);
-> Then I generate the public key:
uint8_t ALL_EVENTS[8]={0x9F,0x01,0x00,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);
ret = hci_le_read_local_p256_public_key();
-> Wait for the callback event:
case HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_SUBEVT_CODE:
{
APP_DBG_MSG("==> OOB Key Gen Event!\r\n");
runOOB();
}
-> runOOB function to set the OOB data in the NFC tag:
static void runOOB(void)
{
uint8_t at = 0;
uint8_t add[6] = {0,0,0,0,0,0};
uint8_t len = 0;
uint8_t rand[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
uint8_t hash[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
ST25DVxxKC_PASSWD_t default_password = {.MsbPasswd=0, .LsbPasswd=0};
ST25DVxxKC_RF_PROT_ZONE_t rf_write_protect = {.PasswdCtrl = ST25DVXXKC_PROT_PASSWD1 , .RWprotection =ST25DVXXKC_WRITE_PROT};
NFC07A1_NFCTAG_SetRFDisable_Dyn(0);
NFC07A1_NFCTAG_PresentI2CPassword(0, default_password);
NFC07A1_NFCTAG_WriteRFZxSS(0, ST25DVXXKC_PROT_ZONE1, rf_write_protect);
/* This dummy call is required to enable OOB */
#ifdef OOB_SECURE
int status = aci_gap_set_oob_data(0,0,add, 0, 0, rand);
#endif
Ndef_Bluetooth_OOB_t NdefBle = {
.OptionalMask = (NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_COMPLETE_LOCAL_NAME) |
NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_SECURITY_MANAGER_TK_VALUE)),
.LocalName = "ST25OOB",
.Type = NDEF_BLUETOOTH_BLE,
.Role = NDEF_BLE_ROLE_PERIPH_ONLY,
.DeviceAddressType = NDEF_BLE_PUBLIC_ADDRESS_TYPE
};
#ifndef OOB_SECURE
memcpy(NdefBle.DeviceAddress,bd_addr_udn,sizeof(NdefBle.DeviceAddress));
for(int i = 5; i >= 0; i --)
NdefBle.DeviceAddress[i] = bd_addr_udn[5-i];
#else
status = aci_gap_get_oob_data(1, &at,add,&len, rand);
status = aci_gap_get_oob_data(2, &at,add,&len, hash);
for(int i = 5; i >= 0; i --)
NdefBle.DeviceAddress[i] = add[5-i];
for(int i = 15; i >= 0; i --)
{
NdefBle.SimplePairingRandomizer[i] = rand[15-i];
NdefBle.SimplePairingHash[i] = hash[15-i];
}
#endif
NDEF_ClearNDEF();
NDEF_AppendBluetoothOOB(&NdefBle, "STM32WBA52");
NFC07A1_NFCTAG_ResetRFDisable_Dyn(0);
LOG_INFO_APP("==> Run OOB Function Executed!\r\n");
//BSP_LED_On(LED_BLUE);
}
This should allow to bluetooth pair by tapping the NFC tag with the phone, however it is requiring a pin as if it was using only the I/O capability (display one). Can anyone provide solutions?
Best regards.
2024-04-15 8:45 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.