2024-04-04 1:19 AM
Everywhere I look it is written to be 30 seconds.
But Its too much time for me, Is there a parameters in Init or during connection I can change?
2024-04-15 8:48 AM
Hello @DS.4 ,
The default GATT timeout is often set to 30 seconds, which is a balance between allowing enough time for a device with potentially slow communication and not waiting excessively long for a response. However, the timeout duration is not standardized and can vary depending on the implementation of the Bluetooth stack on the devices involved.
Remember : that setting the timeout too short might lead to unintended disconnections, especially in environments with interference or when communicating with devices that have slower response times. Always consider the trade-offs when adjusting such parameters.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.