2024-02-21 6:00 AM
Hello,
I used the onboard ST-Link Debugger of the STM32F401RE to flash/debug external boards. Can I do the same with the Nucleo-STM32WL55JCx Board(using the MIPI10 Connector)?
I checked UM2592, and it only gives directions about using an external debugger(and turning off the on-board one).
Thank you
Amir
2024-04-15 6:02 AM
Hello @AElgh
yes, you can use the Onboard ST-Link Debugger of the STM32F401RE as an external debug tool to program the on-board STM32WL.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-15 6:05 AM - edited 2024-04-15 6:08 AM
I think @AElgh was asking the opposite question?
ie, can the on-board ST-Link of the Nucleo-STM32WL55JCx be used to program/debug an external target?
2024-04-15 6:12 AM
@STTwo-32 exactly as Andrew said, I wanted to use the on board ST-Link of the nucleo STM32WL to debug other boards (using the MIPI10 Connector)
2024-04-15 7:14 AM
I think that is not possible. There are no jumpers to disconnect SWD/SCK from the on board target as on the stlinkv2 boards.Maybe it can work, if both on board and external target have a ADI DP V2 debug unit, Then maybe multi-drop can work.
2024-04-15 7:47 AM
Hello @AElgh
Sorry for this Mistake, you can't use the on-board ST-Link of the STM32WL Nucleo Board to flash/debug external boards.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-15 8:18 AM
That's a shame.
Was there a reason for removing this useful feature from this board?
2024-04-15 8:27 AM
@STTwo-32: Are you sure that Multidrop does not work? Multidrop must be implemented to talk to both CPUs e.g. on the WL55.
2024-04-15 8:42 AM
That may work. But we can't guarantee.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.