cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55RGV6 (board P_NUCLEO_WB55) STM32cubeprogrammer errors show: first erro: No STM32 target found when i press button 'reset' error: ST_link erro(DEV_TARGET_CMD_ERR) stm32cubeide errors: error in launch sequence: Failed to startGDB server

Lep
Senior

Note: I can use stlink to download programs to other boards.But p_nulceo_wb55 doesn't work well. I use an external stlink instead of the on-board stlink, the errors are same.

I was learning Bluetooth, It would have worked well. After a while, an error has occurred.

Is it because I have downloaded some program?

The errors are as follows(use stm32cubeprogrammer :(

0693W00000NpzZQQAZ.pngthe erros in stm32cubeide:

0693W00000Npzb7QAB.png 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hello,@Sara BEN HADJ YAHYA (ST Employee)

I have posted a lot about these problems, and these methods are not working.I only remember downloading the BLE example at the time, and then the next day there was this failure.

Thanks,

Lep

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.