2022-12-25 7:44 AM
i'm using a NUCLEO STM32WB55RG-D01 eval board.
BLE_HeartRateFreeRTOS sample and my test app were working fine.
after some time of development my test app i found
to check whether it's related with my test app i switched back to the (unchanged) sample app : BLE_HeartRateFreeRTOS : also there i still see it advertising but trying to connect always runs into timeout (same symptoms as with my app).
what migth be broken and why ? what can i do to check (and possibly fix) why it is failing now even with the unchanged sample apps .
other (non BLE) functionality is still running fine.
stepping in the debugger i see no trouble even the connection callback gets called when i try to connect ...
thx, peter
2022-12-25 8:13 AM
just after posting it looks as if i've find the reason.
it seems to be IOS (my test devices) related :they reported that the BLE device lost pairing information and so refused to connect again.
so, i had to fix this on IOS side. (clear pairing information)
peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.