NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Please suggest me some documents explain about RadioSetRxDutyCycle.Thanks.
Hello everyone. 4 years ago i began developing a project from this board B-L072Z-LRWAN1 using a LoRa "PingPong" example. Now i want to re-start this project on Nucleo-STM32WL55, but there is not a "LoRa PingPong" example, only a SubGhz PingPong (alas...
HiWe have a project that uses the STM32WB55 with the full BLE stack in version 1.10.1. Today I recorded some air traffic between my PC and the device and struggled over something that confused me.In our project we have disabled the data length suppor...
Hello,I am having trouble running a successful LoRaWAN FUOTA campaign for my Nucleo-WL55JC development board. I am using the LoRaWAN_FUOTA_DualCore example project found in the STM32CubeWL_V1.2.0 firmware package, and am using AWS-IoT for LoRaWAN as ...
Hi,On a custom board I can no longer reprogram the MCU (STM32WB15) via the SWD link.The last program flashed on the card works perfectly but I can no longer establish the SWD link with CubeIde via the ST-LINK probe.Message "target not found".I guess ...
I'm developing my custom board using a STM32WB55VGY6TR microcontroller and I want to use the Nucleo-WB55 developer kit as a programmer for my custom circuit board.However, I cannot start debugging using STM32cubeIDE. The IDE said that failed to start...
Hello,In STM32WLE5CC Lorawan, when It Doesn't get ack for confirmed uplink, it decreases its datarate(Increase SF), but not TX Power is increases.Say Due to ADR Device is at DR5 and TX Power 10. Due to increase in noise, device doesn't get ack from L...
I connected a LED to the PA11 pin of STM32WB55VGY microcontrollerand I want to toggle it.So, I'm trying to use HAL_GPIO_TogglePin(xx, yy) but I cannot know the "xx (GPIO_Typedef)" of PA11 pin.Where can I found which pin is which GPIOx?
Hi,I am developing a small module with the STM32WB10 and I need to do 10 ADC conversions (9 external and the internal temperature).However, I can only get the DMA to do the 8 channels configured in the regular channel ranks (Number of conversions = 8...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.