2025-05-18 4:01 AM
Hi,
I have to use the transceiver for pure RF communications and implement my own protocole.
After checking several boards, I've be recommended the P-NUCLEO-WB55 but from all the doc and example I find, the transceiver is used for BlueTooth communications, which I don't need at all.
Is it possible to use its transceiver RF without BLE, Zigbee, etc... as a simple 2.4Ghz range transmitter and receiver?
If not, which MCU should I get, that includes a dev board offering AD, DA and pure RF ?
Thanks for any light.
Steve
Solved! Go to Solution.
2025-05-19 1:41 AM
Hello,
you can create your own protocol built on 802.15.4.
Please have a look here for more information.
Connectivity:Introduction to 802 15 4 - stm32mcu
Best regards,
ST support
2025-05-19 1:41 AM
Hello,
you can create your own protocol built on 802.15.4.
Please have a look here for more information.
Connectivity:Introduction to 802 15 4 - stm32mcu
Best regards,
ST support
2025-05-19 2:13 AM
@SteveJ wrote:If not, which MCU should I get, that includes a dev board offering AD, DA and pure RF ?
Does the RF need to be 2.4GHz ?
2025-05-19 2:49 AM
Andrew,
Yes it has to be in the 2.4GHz range, not sub GHz.
Steve
2025-05-19 2:51 AM
Hello @SteveJ
As suggested by @FilipKremen, the 802.15.4 is a widely used communication protocol that enables the creation of Wireless Personal Area Networks (WPAN). So, it will be a good idea to use it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.