2025-03-19 6:34 AM - last edited on 2025-04-28 7:03 AM by STTwo-32
Hi,
I have attached a X-NUCLEO-WB05KN1 on top of a NUCLEO-H743ZI2 board and are trying to verify whether it works by flashing the peripheral_hr sample with the shield argument "x_nucleo_wb05kn1_spi". Sadly it does not work (it is stuck in bt_spi_open when trying to receive SPI header from shield)
The shield is flashed such that it uses SPI instead of UART.
I have done the same experiment, placing the shield on top of Nordic Semiconductors' nRF52840 MCU and here it works with the peripheral_hr sample with shield argument.
I have also tried the experiment on a NUCLEO-F401RE and here it also fails.
Any ideas what could be wrong?
2025-03-23 11:34 PM
Any updates?
2025-04-28 5:48 AM - edited 2025-04-28 5:56 AM
Hello @CBras
This behavior has been escalated internally (under internal ticket number 208694). I will get back to you ASAP.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-16 9:01 AM
I'm experiencing the same issue
2025-05-18 10:08 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.