2025-02-25 7:20 AM
hello
I'm working on a STM32WB55 P-NUCLEO
I'm trying to make a binary that will self update Wireless stack (WL FW
I took inspiration from https://github.com/stm32-hotspot/STM32WB-FUS-Command-Line-Interface.git
the objective is to embed new FW in a C byte array and to let the user binary to call FUS for :
delete current stack
calc the good adress for WL FW (@SFSA -
clean flash
copy the new WL FW C blob
call upgrade
all the rest is ignored right now to simplify explainations
here you can find my app_entry.c APPE_SysEvtReadyProcessing function (everything is here)
static void APPE_SysEvtReadyProcessing(void * pPayload)
{
uint8_t fus_state_value;
SHCI_CmdStatus_t res;
TL_AsynchEvt_t *p_sys_event;
SHCI_C2_Ready_Evt_t *p_sys_ready_event;
SHCI_FUS_GetState_ErrorCode_t ec;
p_sys_event = (TL_AsynchEvt_t*)(((tSHCI_UserEvtRxParam*)pPayload)->pckt->evtserial.evt.payload);
p_sys_ready_event = (SHCI_C2_Ready_Evt_t*) p_sys_event->payload;
/* Traces channel initialization */
TL_TRACES_Init();
FLASH_OBProgramInitTypeDef ob;
HAL_FLASHEx_OBGetConfig(&ob);
start_fw_address=ob.SecureFlashStartAddr-(((BIN_SIZE/FLASH_PAGE_SIZE)+1)*FLASH_PAGE_SIZE); // @of first flash page that fits the FW size
uint8_t FUS_FW_RUN=!(p_sys_ready_event->sysevt_ready_rsp == WIRELESS_FW_RUNNING);
if (!FUS_FW_RUN){
APP_DBG_MSG("[-- WIRELESS FW IS RUNNING --]\r\n");
printf("WIRELESS FW running reboot to FUS\r\n"); HAL_Delay(100);
(void)SHCI_C2_FUS_GetState( NULL );
(void)SHCI_C2_FUS_GetState( NULL );
wait4reboot();// this is and infinite while with a refresh of IWDG
}
else
{
APP_DBG_MSG("[-- FUS IS RUNNING --]\r\n");
printFusNWirlessInfos(); // display wireless firmware version / build / type
printFWpointers(); // display differentes usefull adress (app / wl / sfsa etc.)
fus_state_value = SHCI_C2_FUS_GetState( &ec );
while(fus_state_value != FUS_STATE_VALUE_IDLE){
printf("FUS PROCESS on going ... ");
print_FUS_STATE_VALUE(fus_state_value,ec); // display FUS state and error status
fus_state_value = SHCI_C2_FUS_GetState( &ec );
HAL_Delay(500);
}
print_FUS_STATE_VALUE(fus_state_value,ec);
switch(CFG_REBOOT_VAL_MSG)
{
case CFG_IDLE:
printf("START UPDATE PROCEDURE\r\n");
CFG_REBOOT_VAL_MSG=CFG_FUS_FW_DELETE;
wait4reboot();
break;
case CFG_FUS_FW_DELETE:
printf("DELETE CURRENT FUS FIRMWARE\r\n");HAL_Delay(500);
printf("call SHCI_C2_FUS_FwDelete()\r\n");HAL_Delay(500);
res =SHCI_C2_FUS_FwDelete();
if(res==SHCI_Success){
CFG_REBOOT_VAL_MSG = CFG_FUS_FW_UPGRADE;
print_SHCI_CmdStatus_t(res);HAL_Delay(100);
wait4reboot();
}
else{
CFG_REBOOT_VAL_MSG = CFG_IDLE; // back to begining
print_SHCI_CmdStatus_t(res);HAL_Delay(100);
wait4reboot();
}
break;
case CFG_FUS_FW_UPGRADE:
APP_DBG_MSG("UPGRADE WIRELESS FIRMWARE\r\n");
Delete_Sectors();
copyBin();
checkBin();
printf("call SHCI_C2_FUS_FwUpgrade(0,0)\r\n");
CFG_REBOOT_VAL_MSG = CFG_FUS_END;
res =SHCI_C2_FUS_FwUpgrade(0,0);
print_SHCI_CmdStatus_t(res);HAL_Delay(100);
do{
printf("UPGRADE ongoing ... ");
fus_state_value = SHCI_C2_FUS_GetState( &ec );
print_FUS_STATE_VALUE(fus_state_value,ec);
HAL_Delay(500);
}while(1);//while(fus_state_value != FUS_STATE_VALUE_IDLE);wait4reboot();
break;
case CFG_FUS_END:
APP_DBG_MSG("END OF PROCESS\r\n");
CFG_REBOOT_VAL_MSG = CFG_IDLE;
wait4reboot();
break;
default :
CFG_REBOOT_VAL_MSG = CFG_IDLE;
break;
}
}
wait4reboot();
}just here you can find the output durring all process over all reboots
[-- FUS IS RUNNING --]
Get Wireless Infos : SHCI_Success
Wireless Firmware version 0.0.0 // no WL stack installed yet
Wireless Firmware build 0
FUS version 1.2.0
Wireless Firmware Type : Unknown
StartOfAppAddr : 0x08000000 // this user app
EndOfAppAddr : 0x0803E800
SecureFlashStartAddr : 0x080F4000 // SFSA addr
StartOfFwPageAddr : 0x080D0000 // calc addr of newly installed WL stack ( based on SFSA)looks coherent with readme of STM32CubeWB release
SizeOfFW : 0x00023F80 // size of new WL stack
EndOfFwAddr : 0x080F3F80 // las WL stack @ (muste be less that actual SFSA)
FUS state : IDLE | FUS_STATE_ERROR_NO_ERROR
START UPDATE PROCEDURE
[-- FUS IS RUNNING --] // first manual reboot to trigg the start sequence
Get Wireless Infos : SHCI_Success
Wireless Firmware version 0.0.0
Wireless Firmware build 0
FUS version 1.2.0
Wireless Firmware Type : Unknown
StartOfAppAddr : 0x08000000
EndOfAppAddr : 0x0803E800
SecureFlashStartAddr : 0x080F4000
StartOfFwPageAddr : 0x080D0000
SizeOfFW : 0x00023F80
EndOfFwAddr : 0x080F3F80
FUS state : IDLE | FUS_STATE_ERROR_NO_ERROR
DELETE CURRENT FUS FIRMWARE
call SHCI_C2_FUS_FwDelete() // clear actual WL stack
SHCI_Success
[-- FUS IS RUNNING --] // reboot trigged by FUS after SHCI_C2_FUS_FwDelete()
Get Wireless Infos : SHCI_Success
Wireless Firmware version 0.0.0
Wireless Firmware build 0
FUS version 1.2.0
Wireless Firmware Type : Unknown
StartOfAppAddr : 0x08000000
EndOfAppAddr : 0x0803E800
SecureFlashStartAddr : 0x080F4000
StartOfFwPageAddr : 0x080D0000
SizeOfFW : 0x00023F80
EndOfFwAddr : 0x080F3F80
FUS PROCESS on going ... FUS state : SERVICE_ONGOING | FUS_STATE_ERROR_IMG_NOT_FOUND // ok because no WL is installed yet (problem is the same if I avoid this step)
FUS state : IDLE | FUS_STATE_ERROR_NO_ERROR
UPGRADE WIRELESS FIRMWARE
Erasing internal memory sectors [62 244] // errase flash (even if it should ne be needed)
OK
flash wireless FW @ 0x080D0000 // copy C byte array to the
OK
[AB A3 2C F4 ... 22 5E 2C A1 D3 ] // check that flash is ok regarding the input C byte array
Check Copy FW from: 0x080D0000 to : 0x080F3F80
0 err found // no error durring flash
call SHCI_C2_FUS_FwUpgrade(0,0)
SHCI_Success
[-- FUS IS RUNNING --] // reboot trigget by FUS right after SHCI_C2_FUS_FwUpgrade call
Get Wireless Infos : SHCI_Success
Wireless Firmware version 1.21.0 // WL stack looks to be found
Wireless Firmware build 3
FUS version 1.2.0
Wireless Firmware Type : Unknown
StartOfAppAddr : 0x08000000
EndOfAppAddr : 0x0803E800
SecureFlashStartAddr : 0x080D0000 // SFSA looks to be well moved to the new WL Stack place
StartOfFwPageAddr : 0x080AC000 // not relevant yet as SFSA is including new WL stack
SizeOfFW : 0x00023F80
EndOfFwAddr : 0x080CFF80
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR // FUS stil in upgrade
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_NO_ERROR
[-- FUS IS RUNNING --] // new reboot triged by FUS
Get Wireless Infos : SHCI_Success
Wireless Firmware version 0.0.0 // WL stack looks empty now
Wireless Firmware build 0
FUS version 1.2.0
Wireless Firmware Type : Unknown
StartOfAppAddr : 0x08000000
EndOfAppAddr : 0x0803E800
SecureFlashStartAddr : 0x080F4000 // SFSA get back to "no WL stack" position
StartOfFwPageAddr : 0x080D0000
SizeOfFW : 0x00023F80
EndOfFwAddr : 0x080F3F80
FUS PROCESS on going ... FUS state : FW_UPGRD_ONGOING | FUS_STATE_ERROR_IMG_CORRUPT // ???
FUS state : IDLE | FUS_STATE_ERROR_NO_ERROR
END OF PROCESSmy issue is that even if at beginig new WL stack looks to be well discovered after fus upgrade call I got a new reboot with a "fus error image corrupted" even if I have well check my copy in flash
I did succeded few times to get this WLStack accepted by fus I didn changed anything to my byte array
heres my WL stack byte array files
#ifndef _BIN_IMAGE_H_
#define _BIN_IMAGE_H_
/***************************************************************************//**
* file ./bin_image.h
* Binary FW file to H file converter
* Generated on February 25, 2025 at 15:38:02
******************************************************************************/
#include <stdint.h>
/* stm32wb5x_BLE_Stack_full_fw.bin */
#define FW_DATETIME "February 25, 2025 at 15:38:02"
#define FW_NAME "stm32wb5x_BLE_Stack_full_fw.bin"
#define BIN_SIZE 0x23f80
extern const uint8_t FW_Bin[BIN_SIZE];
#endif //_BIN_IMAGE_H_/***************************************************************************//**
* file ./bin_image.c
* Binary FW file to C file converter
* Generated on February 25, 2025 at 15:38:02
******************************************************************************/
#include <stdint.h>
#include "bin_image.h"
/* stm32wb5x_BLE_Stack_full_fw.bin */
const uint8_t FW_Bin [BIN_SIZE] = {0xab,0xa3,0x2c,0xf4,0x2,0x4a,0x25,0x30,0x9f,0x76,0xfd,0x2f,0x1e,0x36,0x15,0x0,
// reduced to not overtflow the forum
0x45,0x0,0x11,0x22,0x5e,0x2c,0xa1,0xd3,};my c bytes array representing the new Wireless FW is generated by a really simple python script
if anyone has an idea why I got this corrupted image error I'm more that happy to read it !
thanks a lot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.