2021-01-01 3:12 PM
Is it possible to use MCUs in the STM32WB line in both Bluetooth LE and Bluetooth Classic modes at the same time? I've seen that it does "dual mode", but not whether it can do both at the same time.
Thanks
Solved! Go to Solution.
2021-01-22 6:41 AM
STM32WB is offering a set of low power modes that would not fit with the BLE Classic consumption requirements.
This is why it only targets low energy protocols: BLE, BLE Mesh, Thread, Zigbee, 802.15.4.
Only some dual low energy protocol modes are supported: "BLE + Thread" now and "BLE + 802.15.4" in the coming weeks.
2021-01-22 6:41 AM
STM32WB is offering a set of low power modes that would not fit with the BLE Classic consumption requirements.
This is why it only targets low energy protocols: BLE, BLE Mesh, Thread, Zigbee, 802.15.4.
Only some dual low energy protocol modes are supported: "BLE + Thread" now and "BLE + 802.15.4" in the coming weeks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.