2020-10-05 8:37 AM
Hello,
is there anyway to get an event or interrupt, after the transmission is finished of each packet from Advertising. I know this depends on Intervals Min and Max buti don't want to make a timer to syncronize an interrupt with the intervals. Thanks.
2020-10-14 7:09 AM
Aci_hal_set_radio_activity_mask(0x0002) bitmask of advertising can be used to detect the end of advertising phase.
The ACI_HAL_END_OF_RADIO_ACTIVITY_EVENT is generated at the end of each radio activity and so at the end of the last advertising packet during the advertising phase.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.