2020-09-24 6:57 AM
Hello,
I am trying to use the STM32WB55 Nucleo Pack to develop a BLE application.
Does anyone know what these constants represent ?
/**
* There is one handler per service enabled
* Note: There is no handler for the Device Information Service
*
* This shall take into account all registered handlers
* (from either the provided services or the custom services)
*/
#define BLE_CFG_SVC_MAX_NBR_CB 7
#define BLE_CFG_CLT_MAX_NBR_CB 1This code is extracted from the client project but it is the same in the server project.
Thank you for your reply!
2020-10-14 8:13 AM
These 2 constants are initialized by the BLE controller:
Regarding BLE_CFG_SVC_MAX_NBR_CB :
This API registers a handler to be called when a GATT user event is received from the BLE core device. When
/* a Service is created, it shall register a callback to be notified when a GATT event is received from the
* BLE core device. When a GATT event is received, it shall be checked in the handler if the GATT events belongs
* to the Service or not. The handler shall return the correct status depending on the result. As soon as one
* Service handler registered acknowledges positively the GATT event, the ble_controller stops calling the
* registered Service handlers. */
void SVCCTL_RegisterSvcHandler( SVC_CTL_p_EvtHandler_t pfBLE_SVC_Service_Event_Handler )
{
#if (BLE_CFG_SVC_MAX_NBR_CB > 0)
SVCCTL_EvtHandler.SVCCTL__SvcHandlerTab[SVCCTL_EvtHandler.NbreOfRegisteredHandler] = pfBLE_SVC_Service_Event_Handler;
SVCCTL_EvtHandler.NbreOfRegisteredHandler++;
#else
(void)(pfBLE_SVC_Service_Event_Handler);
#endif
Then the handler is registered during the initialization of the service.
/**
* Register the event handler to the BLE controller
*/
SVCCTL_RegisterSvcHandler(PeerToPeer_Event_Handler);
It is the same for BLE_CFG_CLT_MAX_NBR_CB
SVCCTL_RegisterCltHandler() is used for clients
SVCCTL_RegisterSvcHandler() is used for services.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.