2021-04-09 10:10 AM
STM32CubeMonRF: https://www.st.com/en/development-tools/stm32cubemonrf.html
Seems to apply to BLE and IEEE 802.15.4 only?
Is there anything similar for sub-GHz ?
2021-04-15 1:08 AM
Hello
You are right, STM32CubeMonitor-RF is supporting the STM32WB series, and then covering only BLE and 802.15.4.
For sub-GHz, there are similar functions for RF tests with STM32WL, but there are covered by STM32CubeMonitor and specific STM32WL flows. It is described in this wiki : https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:Wireless_Long_Range_RF_Test
The flows are included in STM32WL Cube firmware.
Best regards
2021-04-15 7:07 AM
Thanks.
Is that facility also available with other non-WL sub-GHz products?
2021-04-15 7:14 AM
Right now, it seems that only the STM32WL package have a demo and RF test dashboard for CubeMonitor.
2021-04-15 7:28 AM
In principle, should it work with others?
Or is there some specific tie to the WL ?
2021-05-03 6:36 AM
Hello Andrew.
The STM32WL RF test panel uses AT commands available on STM32WL. As it is non standard commands, it is unlikely to work other product.
Stephane
2021-05-04 7:36 AM
I see.
:\
Any plans to make such a thing available for other sub-GHz products?
2021-05-04 8:05 AM
What sub-Ghz products do you have in mind ?
2021-05-05 3:48 AM
At this moment, B-L072Z-LRWAN1
In general:
Your SPIRIT range?
I-NUCLEO-LRWAN1
etc, etc, ...
https://www.st.com/en/wireless-connectivity/proprietary-sub-1-ghz-products.html
2021-05-05 10:34 AM
Hello Andrew
The AT commands of I-CUBE_LRWAN looks similar to the one used on STM32WL, but not fully identical.
I assume it may not work with your board and there is no plan to adapt the STM32WL flow.
( With STM32CubeMonitor editor, you can edit the flow to adapt it to you need).
Best regards
Stephane
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.