NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using SAI protocol to get the audio output...For now I am directly using the bin file provided in the sample code...I just wanted to know if we have mp3 file or any other format other then bin file, how it can be dumped to board using STM32CubeP...
Dear Hosts! I seem to have a problem joining the meeting. The link I recieved is not working. Yesterday I had no problem with joining the help-me session. Could you please resend the link to me?
Morning, I cannot find the link to join. Please resend
Hi -- AN5434 refers to using the MB1623 MCU reference design board with several add-on antenna PCBs without specific PCB part numbers, but AN5434 links only to a PDF and it doesn't include either all the needed antenna trace / PCB CAD dimensions or a...
Hello all,Thanks for your supportI'm using STM32WB55cc MCU and I want to read the LDR and PIR sensor value using ADC. In ADC1, channel 6 (CH6), channel 11(CH11) are using. how to configure and read the data From ADC1. NOTE: STM32WB55cc MCU has a sing...
I am using B-L072Z-LRWAN1. I ran the ping pong application ready here. I wanted to set up timer interrupt myself but there is no .ioc file. I opened another project, set up a timer in cubemx, tried and run it, and added it to the ping pong project. b...
We figure that the STM32WB55 support only sending audio data through opus codec and doesn't have an A2DP behavior like other traditional BL. Could integrate an audio profile to the STM32WB for MP3, AAC, WAV
Hi, I am using STM32WB55RG as the MCU and LSM6DSO32 as the ACCELEROMETER in my project. In order to get my project CE certified, I require the Certificate Of Conformity for the both components.Hope you guide me to the right path.Thank You and Warm Re...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.