cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK-V3PWR

Karthi
Associate II

 STLINK-V3PWR Not able to connect to STM32WL and other STM32 MCU's using STM32CubeProgrammer

Same MCU is working with STlink-V3

 13:39:13 : ST-LINK SN : 002F004D3431510137383732

 13:39:13 : ST-LINK FW : V4J2B1P4

 13:39:13 : Board    : STLINK-V3PWR

 13:39:13 : Voltage   : 0.02V

 13:39:13 : Error: No STM32 target found

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

Apparently the measured Target MCU voltage is 0.02V, maybe there are some jumpers of switch to adjust to get setup working well.

Karthi
Associate II

Hi

I able to connect now using CubeProgrammer, After connecting TVCC to Target MCU VCC.

Without connecting TVCC to MCU VCC , STlink-V3 is working but not with V3PWR.

again V3PWR is still not working with CubeMX IDE.

Thanks

KarthiG

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.