2025-08-20 2:08 PM
Hello,
I'm trying to figure out why setting the MTU stops the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event from ever firing. This essentially breaks everything.
case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
/* USER CODE BEGIN EVT_LE_CONN_COMPLETE */
hci_le_set_data_length(tpms_handleNotification.ConnectionHandle, /*tx_octets*/251, /*tx_time*/2120);
tBleStatus result = aci_gatt_exchange_config(tpms_handleNotification.ConnectionHandle);
if(result != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("\r\n\r** MTU failed to set.\n\r");
}
/* USER CODE END EVT_LE_CONN_COMPLETE */
/**
* The connection is done,
*/
connection_complete_event = (hci_le_connection_complete_event_rp0 *) meta_evt->data;
BleApplicationContext.BleApplicationContext_legacy.connectionHandle = connection_complete_event->Connection_Handle;
BleApplicationContext.Device_Connection_Status = APP_BLE_CONNECTED_CLIENT;
/* CONNECTION WITH CLIENT */
APP_DBG_MSG("\r\n\r** CONNECTION COMPLETE EVENT WITH SERVER \n\r");
handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT;
handleNotification.ConnectionHandle = BleApplicationContext.BleApplicationContext_legacy.connectionHandle;
P2PC_APP_Notification(&handleNotification);
result = aci_gatt_disc_all_primary_services(BleApplicationContext.BleApplicationContext_legacy.connectionHandle);
if (result == BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("\r\n\r** GATT SERVICES & CHARACTERISTICS DISCOVERY \n\r");
APP_DBG_MSG("* GATT : Start Searching Primary Services \r\n\r");
}
else
{
APP_DBG_MSG("BLE_CTRL_App_Notification(), All services discovery Failed \r\n\r");
}
break; /* HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE */Both the server and client have their, CFG_BLE_MAX_ATT_MTU set to 156. I receive the event and checking the returned value is 156. All of that seems to be working fine.
case ACI_ATT_EXCHANGE_MTU_RESP_VSEVT_CODE:
{
aci_att_exchange_mtu_resp_event_rp0 *exchange_mtu_resp = (aci_att_exchange_mtu_resp_event_rp0 *)blecore_evt->data;
APP_DBG_MSG("**MTU_size = %d \n",exchange_mtu_resp->Server_RX_MTU );
APP_DBG_MSG("\r\n\r");
uint16_t Att_Mtu_Exchanged;
if (exchange_mtu_resp->Server_RX_MTU < CFG_BLE_MAX_ATT_MTU)
{
Att_Mtu_Exchanged = exchange_mtu_resp->Server_RX_MTU - 3;
}
else
{
Att_Mtu_Exchanged = CFG_BLE_MAX_ATT_MTU;
}
}
break;If I comment out these lines, I can receive 20 bytes all day long.
hci_le_set_data_length(tpms_handleNotification.ConnectionHandle, /*tx_octets*/251, /*tx_time*/2120);
tBleStatus result = aci_gatt_exchange_config(tpms_handleNotification.ConnectionHandle);
if(result != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("\r\n\r** MTU failed to set.\n\r");
}With those lines in place, the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event is never fired. This seems to be relevant because when that event isn't fired, the connection handle is never set.
aP2PClientContext[index].connHandle= handle;I'm leaning towards some kind of timing issue because if I set breakpoints and debug, everything magically works, and I can receive more than 20 bytes.
Is there an event I need to catch, should the MTU code be placed somewhere else or am I just thing about/doing this completely wrong?
Any insight would be greatly appreciated.
Kindest regards.
PS. I've reviewed the, BLE_DataThroughput application, now that's an entirely different beast, as well as PM0271. There was also another document I looked at from another post where the OP was having difficulties with setting the MTU as well. None of the searches for setting the MTU really had any resolutions.
2025-09-22 7:02 AM
Hello @kumaichi
Have you tried to debug your code and check where the issue is Happening exactly.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.