2021-09-27 6:19 AM
Hi,
I want to set a publish address in node-1 in BLE mesh without using the mobile app. This address can be either unicast address of other node or group address. Node-2 should be able to receive messages from this node without setting its subscribe address.
In the node-1, I have tried using :
AppliConfigClient_SelfPublicationSet -> ConfigClient_PublicationSet -> ConfigModel_SelfPublishConfig
Here, publish address (unicast address of node-2) is successfully set (checked the return value of the APIs) but publication error occurs on the sw1 press and the node-2 does not receive any message.
I don't want any mobile app intervention after provisioning the nodes.
Which API can be used for my use case ? What am I doing wrong ?
Can I get 'configuration server' code files ? If yes, then how ?
Kindly help me out.
Solved! Go to Solution.
2021-09-28 9:25 PM
Hi, everybody !
I found the solution. Apart from the things I have mentioned above, I enabled the dynamic provisioner in the node-1 and then bound the app key in node-2 (using the mobile app), so now the node-2 is able to receive the messages.
2021-09-28 9:25 PM
Hi, everybody !
I found the solution. Apart from the things I have mentioned above, I enabled the dynamic provisioner in the node-1 and then bound the app key in node-2 (using the mobile app), so now the node-2 is able to receive the messages.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.