NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am working on STM32WB5MMG board and using the example QSPI_ReadWrite_DMA.In the main function the program can not run into case 2 to call HAL_QSPI_Transmit_DMASource Code as below: case 2: if(StatusMatch != 0) { StatusMatch = 0; TxC...
Hi, In my application I have added a custom service with 5 characteristics, all have 128bit UUID, 3 characteristics are 4 byte long and 2 characteristics are 2 byte long.When I compile and connect to board by my phone I can't see the last charactersi...
Hello friends,I am working on STM32WB on-chip Bluetooth low energy system to transmit data from server to client using notification property.I want to transmit 46 bytes at the rate of 500Hz without any packet loss, to achieve this I have updated the ...
Hi,is there anyone who tries to run ota zigbee example? After some debug I think that ota client is unable to write data to flash.From the server side I can see that the process started. From the client side I can see the red led on what mean abort d...
Hi there, I'm struggling with the P-NUCLEO-WB55 kit I just bought...! I wanted to try basic application example given in STM32WB package, followed the documentation and nothing works correctly on the USB dongle...!Application : Zigbee_OnOff_Client_Ro...
Hi all. I'd like to write a simple bare-metal application for STM32WLE5JC. Could you provide snippet code for STM32WL (core + radio) initialization and simple RX/TX Lora Packet ? Thanks Olivier
Note the difference between WB5 and WB55. My main goal is to determine whether I can define any of the pins on the WB5 as SPI or ADC, or are there only certain pins that can perform those functions.
Hello, coming from a STM32L071 + SX1276 application I find it impossible to achieve the equivalent P2P simplicity using the STM32WL package and the latest version of CubeIDE. Am I correct assuming this package only works with the Nucleo hardware at t...
I'm trying to add an external FLASH and RAM to the STM32WB55, but he doesn't have an FMC or FSMC, and all resources a could find related to this subject use the FMC peripheral, there is any way to use the external RAM and FLASH in the same time?shoul...
I am working on smart watch and I have been using STM32WB board, The bluetooth is communicating with the Mic and it is working fine, I want to display, Date and time on my ST7789 display and I want to know how I can display, I am using BLEPeripheral ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.