2024-07-03 4:55 AM - edited 2024-07-03 5:42 AM
Hello,
I am using a Nucleo-WBA52CG dev. board as well as an sd shield.
I want to store data from the NUCLEO in the SD card, and be able to read those data with a computer.
The SD card and the stm32WBA should obviously communicate through SPI.
However, the WBA does not have FatFS, nor SDMMC. I suppose that I can use FileX to partially "replace" those elements, but I see myself unable to find anything related to that situation. I suppose that I'll have to check the custom interface, and as I want to use EXFAT, enable it. But from there I'm kind of lost.
Does anyone have a way to do those communications?
Thanks in advance.
Don't hesitate if you need other informations to facilitate your understanding and give me some hints.
2024-07-04 5:28 AM - edited 2024-07-04 5:33 AM
Hello @Curious_Intern
For the FileX implementation on the Nucleo-WBA52CG, I suggest you take a look at this project to understand how it works.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-04 7:29 AM - edited 2024-07-05 1:04 AM
Hello @STTwo-32, and thank you for your quick answer. It does help to understand the way FileX could be used, but the situation i'm in is different and that difference makes everything trickier haha.
Anyway, do you have any advise about how to link SPI communication and FileX? It seems that in your example everything is done internally but I have to deal with the SD card inherent communication protocol with its own clock etc. (edit: It seems that the "fx_stm32_sram_driver" function play a role in the communication but I could not find it anywhere, in addition to my other questions do you have it somewhere?)
It's been several days since I started doing researches about using an SD Card with FileX without SDMMC or SDIO etc, but I could not find any proper example. And it seems that several developers on ST's Community forum are facing the same issue. Do you have anything resembling something like that?
It would be a great help to me, and others ;)
Thanks a lot anyway, and delighted to learn new thicks thanks to you.
2024-08-06 9:55 AM
unfortunately, there is no such example. What I suggest you is to try to understand how the procedure works from the examples such as the one I've shared with you. then, you can do your own configuration the way you want.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-02 1:30 AM
Have you got the answer of your question?? if yes, then give me the link. I iam also facing trouble as there is no sd card interface i.e fatfs library and no SDMMC option after activating the filex middleware packages in stm32cube MX.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.