2018-03-13 3:07 PM
Hi,
I have b-l072Z-LRWAN1 + SigFox SDR dongle.
I added Node's ID to SENK (network emulator), then I loaded AT command and push button examples from X-CUBE-SFOX, and nothing worked. When I sent a frame, it seems that software gets pending and nothing works again util I reset the device.
Note: I connected JP9 to pin 1 and 2. and PAC is set to Zeros.
Does anyone have an idea about the issue? How can I send it correctly?
Best regards.
#b-l072z-lrwan1 #sigfox2018-03-13 3:13 PM
Note: I also set the key to public key
2018-03-14 9:01 AM
Hello Khaled,
With the AT command example, do you have LED2 blinking when sending AT$SF command?
You should also have an AT reply 'OK' once transmission is done.
On SNEK software, can you try with authentication disabled? This should even work without switching to public key.
Aurelien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.