2024-01-26 8:54 AM
Hi! I have a nucleo WB55 board that I am using for a project. I know with other nucleo boards, it is possible to power them externally with 5V or 7-12V. However, I am not able to verify whether this is possible on the NUCLEO WB55 board, as I can't find the external power supply guidance/instructions in the User Manual.
My aim is to power the board directly with either 12V or 5V but I don't know if this is doable, or the how I could go about it if it is. Please let me know your thoughts.
Solved! Go to Solution.
2024-01-26 10:15 AM - edited 2024-01-26 10:16 AM
Welcome @odianosen_o, to the community!
Yes, you can also supply the NUCLEO-WB55RG externally with 5V or 7...12V. Unfortunately, this has not (yet) been noted in the manuals, but you will find a hint in the schematics (to be found in tab CAD Resources) on page 5: there are two options for the external voltages 5V_EXT (CN7.6) and VIN (CN7.24) on the MORPHO pins.
The MORPHO connections are the external pin rows, which provide significantly more pins than the limited Arduino pins.
Hope that helps?
Regards
/Peter
2024-01-26 10:15 AM - edited 2024-01-26 10:16 AM
Welcome @odianosen_o, to the community!
Yes, you can also supply the NUCLEO-WB55RG externally with 5V or 7...12V. Unfortunately, this has not (yet) been noted in the manuals, but you will find a hint in the schematics (to be found in tab CAD Resources) on page 5: there are two options for the external voltages 5V_EXT (CN7.6) and VIN (CN7.24) on the MORPHO pins.
The MORPHO connections are the external pin rows, which provide significantly more pins than the limited Arduino pins.
Hope that helps?
Regards
/Peter
2024-01-26 10:40 AM
Thanks so much for this! Follow up question based on externally powering the nucleo board. If I want to debug or program the board, would I have to disconnect the external power before plugging in the USB to my PC/ hooking up to ST-Link?
2024-01-26 2:07 PM
No, there‘s a jumper block selecting the supply voltage. Just move it to the required position.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.