STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

End node stm32l073rz and lrwan-ns1 doesn't join

I am using the p-nucelo-lrwan3 and I have been using the i-cube-wl project and i did some changes to the region and to the activation mode but it doesn't join the network can any body help me with it 

Dan33 by Associate II
  • 9876 Views
  • 20 replies
  • 3 kudos

I'm unable to connect to the ZigBee network

I'm trying to create a new ZigBee network frame for STM32WB55RG Zigbee 3 and DIGI Zigbee 3, but it's not working,My request is :How to configure Zigbee network step by stepHow to set unique PAN-IDHow to set 64 bit MAC addressHow to send and Received ...

Hari96 by Associate
  • 1693 Views
  • 1 replies
  • 0 kudos

Power consumption NUCLEO-WL55JC2

Hi, I am trying to measure the power consumption of my NUCLEO-WL55JC2.In the user manual here Is what I found :  Jumper JP1, labeled I_SoC, is used to measure the STM32WL microcontroller consumption by removing thejumper and by connecting an ammeter....

LearnCORE by Associate II
  • 4353 Views
  • 6 replies
  • 1 kudos

Resolved! Pulse sensor and input voltage

Good morning,I am building a system with stm32 wl55jc1 to count water flow with a pulse flow meter.So I created two internal clocks in stm32 one to create a time window and the other that counts each pulse received from the sensor. At the trigger of ...

IngSerio by Associate III
  • 2384 Views
  • 2 replies
  • 1 kudos

SPIRIT library and Sub_GHZ lib compatibilty

Hi A previous version of a product used STM32G071x8/xB in conjunction with external radio transceiver (SPSGRF-915). The team has used SPIRIT middle ware for radio functions. A newer version has migrated to STM32WLE5/E4xx which has inbuilt radio and I...

pavitrar by Associate
  • 1765 Views
  • 2 replies
  • 0 kudos

STM32WB55 ACI_GATT_NOTIFICATION_COMPLETE_EVENT never fired

Hi,I am using aSTM32WB55Wireless Firmware version 1.17.2Wireless Firmware build 1FUS version 1.2.0As described by AN5270 2.5.6. an ACI_GATT_UPDATE_CHAR_VALUE must fire an ACI_GATT_NOTIFICATION_COMPLETE_EVENT if the characteristic was created with GAT...

Resolved! STM32WB5MM-DK unable to connect over Matter

I am attempting to use the https://github.com/stm32-hotspot/stm32wb-matter-device-over-thread/ repo to connect a STM32WB5MMG-DK to an Amazon Alexa acting as a border router, using the Alexa app. The device always fails to connect, outputting the seri...

RHeyse by Associate
  • 5817 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.