2024-11-13 6:14 AM
I use the NUCLEO-WL55JC STM32WL Nucleo-64 board, which I supply with an external power supply.
Each time I attach my laptop in order to view the console, the WL55JC is reset. I assume the STLINK-V3E issues a reset to the WL55JC.
Is there a possibility to avoid that?
I tried to take away the jumper that allows T_NRST to be connected to ST-LINK, but then, when I attach my laptop the board, the WL55JC enters an unusual state (it neither continues normal operation nor does a reset). Except for this I did not find any other ideas how to change the behavior. Is there any?
Solved! Go to Solution.
2024-11-13 7:01 AM
First I left SWDIO and SWCLK, then I removed them. No change.
Yep, a good idea o check the voltages. I'll do that.
2024-11-13 6:18 AM
@HOPilsan wrote:I attach my laptop in order to view the console
What "console" are you using?
2024-11-13 6:26 AM
It is LPUART1 which is tunneled by the ST_LINK through USB to my laptop.
2024-11-13 6:46 AM
Does the board have jumpers/solder-bridges to disconnect the NRST from the ST-Link to the target?
Or use a separate USB-to-UART adaptor.
2024-11-13 6:51 AM
Does the board have jumpers/solder-bridges to disconnect the NRST from the ST-Link to the target?
It does. But as mentioned in the text above I did not get the desired result by removing the jumper. I have no idea why, since this is the obvious approach.
Sure another USB-to-UART adapter could be a solution …
2024-11-13 6:57 AM
@HOPilsan wrote:as mentioned in the text above I did not get the desired result by removing the jumper. …
Sorry - missed that.
Did you leave SWDIO and/or SWCLK connected? Any other connections to the ST-Link?
Do you have a scope to see what's happing on the power lines? Maybe some glitch with power being applied from 2 different sources ... ?
2024-11-13 7:01 AM
First I left SWDIO and SWCLK, then I removed them. No change.
Yep, a good idea o check the voltages. I'll do that.
2024-11-13 9:49 PM
You mentioned you " take away the jumper that allows T_NRST to be connected to ST-LINK", would you confirm which jumper you removed?
BTW, if you assume it's impacted by the NRST, another way is to monitor this signal to see if there is a drop when the reset happens.
2024-11-13 11:56 PM
It was jumper JP8 position 9-10. I'll check both NRST and the voltages and give feedback.
2024-11-14 1:17 AM
Have you checked the RCC_CSR register? It has some bits which identify the cause of a reset...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.