2025-07-12 4:22 AM
Hello ,
I'm trying to flash in the NUCLEO WBA52CG the basic code example available in STM32CubeIDE. I use version 1.19 with Windows. It was originally version 1.17 and was updated in 1.19.
No issue to generate the code or build it. I then connected the NUCLEO WBA52CG and wanted to flash in the board.
I got the failure message "No device found on target."
Can anyone help me ?
I added below a pictures of the connected board. Some leds ( green and red ones) are blinking but I don't know if it's OK or not
Thanks in advance
Regards
Serge
Solved! Go to Solution.
2025-07-17 6:25 AM
Hello
After uninstalling STM32CubeIDE version 1.17 updated in version 1.19 and installing version 1.19 directly from the scratch it’s working fine.
Thank you for your help
Regards,
Serge
2025-07-12 5:03 AM
Hello @Serge1
does it work fine with the STM32CubeProg V2.20.0 (try different mode such as the under reset, normal…).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-14 9:56 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Christian
2025-07-17 6:25 AM
Hello
After uninstalling STM32CubeIDE version 1.17 updated in version 1.19 and installing version 1.19 directly from the scratch it’s working fine.
Thank you for your help
Regards,
Serge
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.