NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I'm currently working on a medical project based on the STM32WB55. One of our key safety requirements is to be able to detect a maximum of clock-related error, including:Complete clock failuresMissed or irregular clock ticksFrequency variations...
I am currently considering capturing and analyzing LE-Audio packets, but for that I need the LTK used for decryption.BLE Secure Connection pairing does not directly exchange LTK, so I do not know what it is, and I am having trouble.Could you please t...
Hi ST Community,I have developed a custom board based on the MB1720 HighBand HighPower A01 reference schematic (STM32WL series). On my custom board, I’m unable to debug the MCU — my debugger can’t connect to the target at all.I’ve double-checked the ...
Dear Team, May I know any hardware design guide exists for STM32WB55RG.Especially for the RF section and it's pch schematic and layout guidelines.RegardsHAI
After I upgraded the FUS version to v2.1.0.0, the STACK version was also upgraded to v1.23.0.3 accordingly, as shown in Figure 1. However, I found that after programming the firmware into the STM32WB55CGU6, I could no longer detect any Bluetooth sign...
Hi, i am currently trying to wrap my head around the OTA Application Update Procedure which STM32 recommends to do.So what i understand is:There is the BLE_Ota example (which basically should take another application binary and write it to some memor...
Hello,I am working with an X-NUCLEO-WB05KN1 expansion board and I need to flash the default DTM firmware into the STM32WB05KN device.In the X-CUBE-WB05N package, I found the following folders:BLE_Transparent_Mode_STM32WB05_controller_onlyBLE_Transpar...
Hi, I am looking for a reference implementation whereby I need to generate a RF carrier wave with 2.45 GHz frequency and also need to variate the Tx output power levels. Is there a sample example to acheive this in Zephyr. My setup:- SW: Zephyr v3.7....
Hi all, I'm fairly new to programming an STM32 :) Is there a simple way of getting started with the above wireless development kit? The documentation on the product page isn't very helpful.
Hello,I am working on a project using the STM32WBA microcontroller and looking for a way to provide Wi-Fi connectivity in order to connect the system to a web server.I've read in several places across ST's website that the STM32WBA series supports Op...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.