2021-06-16 1:51 AM
Hi ,
Default values of the _Min_Heap_Size and _Min_Stack_Size is setting according to What? I changed these variables from 0x200 , 0x400 to 0x00 and 0x00 resprectively ,end then no problem,no error .I guess that Static and dynamic variables in RAM are in the RAM Base Addr + (_Min_Heap_Size or _Min_Stack_Size ) . Why are they 512 byte and 1K byte as default?
Best regards,
Enes.
2021-06-18 2:17 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.