2021-07-08 10:29 AM
if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable)
{
/* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */
/* WARNING: If there is a difference between the MAPPING_TABLE placement in memory */
/* and the address calculated according to the IPCCDBA option byte, */
/* To avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){} */The IPCC addr and MBMUX_ComTable_t value are compared: My results are
IPCCdataBufAddr = 536871136
MBMUX_ComTable_t *pMb_RefTable = 536871140Where do I change this offset value?
2021-07-08 1:51 PM
It references this:
if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable)
{
/* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */
/* WARNING: If there is a difference between the MAPPING_TABLE placement in memory */
/* and the address calculated according to the IPCCDBA option byte, */
/* To avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){} */
2021-07-08 10:21 PM
HI @bblouin
many tips are given in https://community.st.com/s/question/0D53W00000VgqmvSAB/trouble-with-the-stm32cubewl-dual-core-example-projects
1/ Option byte IPCCDBA:
The option byte IPCCDBA probably does not match MAPPING_TABLE address in the linker file at STM32CubeIDE\CM4\STM32WL55JCIX_FLASH.ld.
following rule shall apply IPCCDBA = (MAPPING_TABLE>>4)
please try to program manually option byte IPCCDBA to 0x800. The board will restart to reload the new OB value.
2/
if you are using CubeIDe, you should use the .ld files attached in the post linked above,
please let us know,
2021-07-09 7:27 AM
How do I use STLINK v3 to flash dual-core?
2021-07-09 7:27 AM
How do I use STLINK v3 to flash dual-core?
2021-07-09 7:39 AM
a dual core project is composed of 2 separate projects:
- a cm4 project
- a cm0 project
Compiling a dual core project is nothing else that compiling 2 separate project.
Hence, there will be 2 .elf file generated.
1/ connect to the device using cube programmer (https://www.st.com/en/development-tools/stm32cubeprog.html)
2/For example, you can drag and dorp the 2 elf files into the cubeProgrammer
3/ push download (for both elf) and reset the target.
2021-07-09 10:28 AM
It now says .elf files are too big when I copy/paste.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.