STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Rx timeout on Sub_GHz radio on stm32wle5xx

Here is one problem confused me some days:1. I send some data with LoRaWAN, so it will start RxTimeoutTimer to detect if timeout, and will set radio timeout 0xFFFF as default.2. Normally, the radio will raise IRQ_RX_DONE irq, that mean receive data d...

Zeepunt_0-1720094728355.png
Zeepunt by Associate II
  • 2078 Views
  • 3 replies
  • 0 kudos

ble mesh data reception error

Hi. We are developing a project on STM32WB5MM-DK,BLE-Mesh v1.13.008;BLE-Mesh Library v01.13.009.I'm trying to make a BLOB server model based on an existing stack. I added callback functions and Opcodes_Table . Commands are sent and received (includin...

Resolved! Different behaviour in P-NUCLEO-WB55 boards

We are noticing a difference in the firmware when it is running on the P-NUCLEO-WB55 boardsOn P-NUCLEO-WB55 - MB1355C-02 based evaluation board.- The BLE works correctly. We are able to connect to the device send multiple BLE commands to request the ...

STM32 NUCELO-WBA55CG, No device found on target.

My STM32 WBA55CG was working absolutely fine yesterday and today it seems that, my system refuses to find it. I have checked that i can see it from my device manager but when trying to flash it. It doesn't seem to do anything.When i remove the JP2 ju...

Resolved! B-WL5M-SUBG1 got warning on lorawan app on repo

I tried demo project from repo/STM32Cube_FW_WL_V1.3.0/Projects/B-WL5M-SUBG1/Applications/Lorawan/LoRaWAN_End_Node. i change the Region to my region on Lorawan minddleware setting on CubeMX.After  "debug as" STM32 C/C++ application and got warning "Pr...

flyrobot by Associate II
  • 3566 Views
  • 4 replies
  • 1 kudos

Resolved! HSE with PLL for STM32WB at 64MHZ

There doesn't seem to be any project in the whole STM32CubeWB package that uses the HSE with PLL. At least I couldn't find any with a .IOC file. Most samples in the package use the MSI clock, except, of course, for the wireless projects that use HSE ...

lastMcu by Associate II
  • 3713 Views
  • 6 replies
  • 0 kudos

Resolved! board Suggestion

I was using B-L072Z-LRWAN1 in a project and found out that I needed a very higher transmission rate than LoRa. I am asking if you can suggest me a board that is capable of data transfer rate of 2 Mbps with a duty cycle of 0.2ms. The data size is 30 B...

Sondos by Associate II
  • 2380 Views
  • 4 replies
  • 3 kudos

Resolved! Stm32wb55 custom bluetooth stack

I want to develop my custom bluetooth stack in the stm32wb55 using the rust programming language. Does the st platform allows you to do so? I'm new to the wb wireless microcontroller series and I don't have clear if st allows you to use your own stac...

энн by Associate II
  • 1687 Views
  • 1 replies
  • 0 kudos

Any registers to show receive signal "quality"

For STM32WLE5JCI6TR, is there register on LoRa receiver node to show quality of received signal in1. Slow (for time frame of packet) frequency difference between transmitter and receiver TCXO.2. Fast frequency difference jitter that are at, says, sym...

David_ by Senior
  • 789 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.