2025-09-11 11:09 PM - edited 2025-09-11 11:10 PM
I'm starting a project using the STM32WL55JCI7 chip, but I'm getting the following error. How do I fix this?
An error occurs when compiling with IPCC Activated checked
Description Resource Path Location Type
'IPCC_C2_RX_C2_TX_IRQn' undeclared (first use in this function); did you mean 'IPCC_C1_TX_IRQn'? ipcc.c /STM32WL55JCI7_CM0PLUS/Core/Src line 63 C/C++ Problem
Solved! Go to Solution.
2025-09-15 1:52 AM - edited 2025-09-15 2:32 AM
Hello @haenes_joo
This question has been answered here. If so, please select this post as best answer to close the ticket and give the solution more visibility.
PS: this issue has been also escalated internally to be solved on the future (under internal ticket number 217452).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-15 1:52 AM - edited 2025-09-15 2:32 AM
Hello @haenes_joo
This question has been answered here. If so, please select this post as best answer to close the ticket and give the solution more visibility.
PS: this issue has been also escalated internally to be solved on the future (under internal ticket number 217452).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-23 4:58 PM
Yes, I solved it. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.