2025-09-23 4:56 PM - edited 2025-09-24 8:50 PM
When I run the debugger, it stops at this part and doesn't proceed any further.
void MX_LoRaWAN_Init(void)
-> MBMUXIF_Init();
-> MBMUXIF_WaitCm0MbmuxIsInitialized();
-> void MBMUXIF_WaitCm0MbmuxIsInitialized(void)
{
while (pMb_RefTable->SynchronizeCpusAtBoot != CPUS_BOOT_SYNC_CPU2_INIT_COMPLETED)
{
project : LoRaWAN_End_Node_DualCore
Select radio driver : User board
How do I solve this?
Could something like the above happen if the custom board is not connected properly?
solved it ^^
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.