2020-10-23 6:58 AM
Hello
We are verifying the communication of the IEEE802.15.4 protocol stack with STM32WB50. I tried to insert a 1ms interrupt on CPU1, but when I initialized and enabled IEEE802.15.4, the 1ms interrupt was extended to 2ms. The cause was that the System Clock Mtu input was switched from PLLCLK to HSE_SYS.
The external clock 32MHz is put in the HSE, and the system clock is set to 64MHz by the PLL. And I set the source of System Clock Mtu to PLLCLK.
Please tell me why it switches.
Can the Systemu Clock Mtu source be fixed to PLLCLK?
2020-10-23 10:11 PM
This is the sequel.
After tracking, the SWS / SW of the RCC clock configuration register (RCC_CFGR) changed from 11: PLL selected as system clock to 10: HSE selected as system clock after LL_C1_IPCC_SetFlag_CHx () was called.
I couldn't find such a description in any of the materials.
Why is this happening?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.