2023-02-08 12:04 AM
Kind folks,
STM32Cube IDE newbie here, so please forgive the simple questions.
Context:
I'm trying to create a multi-vendor testbed and diagnostic environment for Matter networks. In the case of ST Micro products, the thought occurs that the two Thread-capable boards in the P-NUCLEO-WB55 pack could form a minimal Thread network, just chatting back and forth between themselves to provide some RF traffic. Idea is to use the demo Thread_FTD_Coap_Multicast application from the STM32CubeWB firmware (v 1.5.0) sample projects, modified to send a packet to its twin based on a timer (instead of user button input).
Questions:
Thanks in advance. Will be happy to share any related results here.
Mike
2023-03-31 5:39 AM
Hello,
1) Yes, you can do that.
2) You can start from Thread_FTD_Coap_Multicast available in STM32CubeWB package v1.16.0.
3) All the data is saved in NVM in internal flash memory. A non-matter device can't communicate with a matter device. The non-matter device will make noise on the channel.
You can find more information regarding matter here and an example stm32wb matter device over thread.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.