STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32CubeProgrammer External Loader issue

Hi!I need to have the ability to program an external SPI flash (W25Q32) via External Loader.I've implemented the loader as described here and it worked successfully for smaller binary file, yet I've got some issues uploading a bigger binary.Once I de...

AZyma.1 by Associate II
  • 2648 Views
  • 2 replies
  • 0 kudos

Why is the SAI (I2S) used in DMA mode generate noise

I am using a SAI device on a SMT32WB55. Using it as a wavetable synth that produces a triangle wave. I am able to play my triangle wave for x amount of time with HAL_SAI_Transmit_DMA(&hsai_BlockA1, (uint8_t*)data, size);And later stop it with a timer...

eeprom by Associate II
  • 2555 Views
  • 3 replies
  • 0 kudos

Resolved! SYSCLK vs SystemCoreClock

Hello,I want to know difference between SYSCLK and SystemCoreClok.When ı try to configure clock of different peripherals I saw terms SYSCLK and SystemCoreClock. I use MSI for SYSCLK which is configured to 32MHZ and for cpu1 ı divided sysclk by 4 and ...

MOB1 by Associate II
  • 4022 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 enable IPCC chage clock and broken usb

I'm generating code with STM32CubeIde 1.11.0 for a STM32WB55, in my test project there is an USB CDC and BLE is enabled.When I enable BLE also IPCC must be enabled, but after HW_IPCC_Init is called usb clock is wrong so my usb device doesn't work any...

juvann by Associate III
  • 2553 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.