2022-10-14 7:07 AM
Hello,
Working on a custom BLE server (peripheral role), I face a trouble exporting the working sources from a Nucleo project (STM32WB55) to a custom board (STM32WB55) project.
Everything is working fine on the Nucleo: advertissing, connection, bidirectional communication etc...
On the custom board, the BLE master sees the advertissing slave, but there is no way to connect to it. It fails connecting!
2 softwares were used on the Master side: ST BLE Toolbox and nRF Connect. Both give same results.
The nRF connect show an additional log error 133(0x85): GATT Error.
The custom board does not implement LSE crystal. HSE is used instead. I follow this URL but cannot find CFG_BLE_LSE_SOURCE in BLE configuration.
(community.st.com/s/article/configuring-stm32wb-for-bluetooth-le-without-an-lse-crystal).
I was expecting a trouble from this point, and found several ticket on the knowledge base, but no one have solution:
- community.st.com/s/question/0D50X0000C3BaK3SQK/migration-from-nucleo-to-my-own-board-doesnt-work
- st.force.com/community/s/question/0D53W000006qrigSAA/stm32wb55-pnucleowb55-advertising-works-but-i-cant-connect-when-building-application-using-code-generated-by-cubemx
No uart debug is possible on the custom board. Is there a way to use custom server application debug trace though STLink/JTAG?
The following items were verified on the custom board:
- Master clock is the expected one, verified on MCO pin.
- The application heartbeat is the expected. The system boot properly as well as the BLE full firmware stack.
- Debugging though STlink/JTAG is working.
- The RTC_WKUP_IRQHandler is verified woked up every 100ms (by toggling a pin).
- The advertising name, device type, tx power level and flags are properly received on the BLE master.
- Connect and Disconnect requests from master trigger the slave to go through Custom_APP_Notification CUSTOM_CONN_HANDLE_EVT and CUSTOM_DISCON_HANDLE_EVT cases on the custom application. This looks like a timeout is triggered on the master, not receiving properly the connection request.
Do you have any clue to help debug the situation?
Solved! Go to Solution.
2022-10-19 12:20 AM
Hello,
Since your custom board doesn't implement LSE, you should use HSE/1024 for RF wakeup clock, and for this, you should enable the calibration for the RF system wakeup clock source in STM32CubeWB package v1.14.1, so you should have this configuration:
/**
* LsSource
* Some information for Low speed clock mapped in bits field
* - bit 0: 1: Calibration for the RF system wakeup clock source 0: No calibration for the RF system wakeup clock source
* - bit 1: 1: STM32W5M Module device 0: Other devices as STM32WBxx SOC, STM32WB1M module
*/
#if defined(STM32WB5Mxx)
#define CFG_BLE_LSE_SOURCE (SHCI_C2_BLE_INIT_CFG_BLE_LSE_CALIB | SHCI_C2_BLE_INIT_CFG_BLE_LSE_MOD5MM_DEV)
#else
#define CFG_BLE_LSE_SOURCE (SHCI_C2_BLE_INIT_CFG_BLE_LSE_CALIB | SHCI_C2_BLE_INIT_CFG_BLE_LSE_OTHER_DEV)
#endifBest Regards
2022-10-19 12:20 AM
Hello,
Since your custom board doesn't implement LSE, you should use HSE/1024 for RF wakeup clock, and for this, you should enable the calibration for the RF system wakeup clock source in STM32CubeWB package v1.14.1, so you should have this configuration:
/**
* LsSource
* Some information for Low speed clock mapped in bits field
* - bit 0: 1: Calibration for the RF system wakeup clock source 0: No calibration for the RF system wakeup clock source
* - bit 1: 1: STM32W5M Module device 0: Other devices as STM32WBxx SOC, STM32WB1M module
*/
#if defined(STM32WB5Mxx)
#define CFG_BLE_LSE_SOURCE (SHCI_C2_BLE_INIT_CFG_BLE_LSE_CALIB | SHCI_C2_BLE_INIT_CFG_BLE_LSE_MOD5MM_DEV)
#else
#define CFG_BLE_LSE_SOURCE (SHCI_C2_BLE_INIT_CFG_BLE_LSE_CALIB | SHCI_C2_BLE_INIT_CFG_BLE_LSE_OTHER_DEV)
#endifBest Regards
2022-10-19 1:14 AM
Dear Remy,
This is it!
Thank you so much.
One thing to take care:
CubeMX generates the SHCI_C2_BLE_INIT_CFG_BLE_LSE_NOCALIB for CFG_BLE_LSE_SOURCE, even when HSE/1024 is seleted.
The correction of the RF system wake up clock source calibration needs to be handled manually after cubeMx code generation, between USER CODE BEGIN/END.
Sincerely
2022-10-19 1:40 AM
Hi,
Yes, you have right, in the next release (v1.15.0), the define CFG_BLE_LSE_SOURCE will be managed by cubeMX according to RF system wake up clock configuration.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.