2019-03-06 12:52 AM
Hello,
I'm using a I-NUCLEO-LRWAN1 shield plugged on a NUCLEO L073RZ board. I'm trying to make the I-CUBE-LRWAN AT-master example run on the Nucleo L073rz. As documentation explain i opened SB13 and SB14 and closed SB62 and SB63, i also redirected the stlink to the uart4 with flying wire to be able to program the board.
To connect to my LoRa server i need to change my DEUI but the shield return an error "ERROR_INVALID_ARGUMENTS" (which is not even in the documentation of the software package) when i try to change it with the AT+EUI=XXXXXXXXXXXXXXXXX command.
Does anyone have any idea on why we can't change the DEUI?
2019-03-06 5:00 AM
According to the USI LoRa manual AT+EUI is a READ-ONLY command, so you're not going to be able to change it.
2019-03-06 5:27 AM
ah yeah ,you're right. it doesn't work the same as in the i-cube-lrwan AT command example that explain a lot... Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.