NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear,I’m working with a B-L072Z-LRWAN1 Discovery Board and AT_Slave sample code of CubeExpansion_LRWAN_V1.2.0.I being able to JOIN to a Gateway, but when I try to send a frame to the Gateway with command AT+SEND= ... , the most of trials I get an A...
After seeing the STM32WB55 series, i want to shift , but it don't have zigbee till now but they mentioned as coming soon? So, will they update it over the internet or using any software? Will it inter-operable with Digi Xbee s2c/Pro module?
Hello,I’m working with a B-L072Z-LRWAN1 Discovery Board and AT_Slave sample code of CubeExpansion_LRWAN_V1.2.0.I being able to JOIN to a Gateway, but when I try to send a frame to the Gateway with command AT+SEND= ... , the most of trials I get an ...
Hello, i am working with this kits and library. Using ping-pong example for learn but now i want to add a new uart then read gps datas and monitor on a screen. CubeMX have B-L072Z-LRWAN1 in board section. But after generate code you have just a idl...
Hello,I'm using a I-NUCLEO-LRWAN1 shield plugged on a NUCLEO L073RZ board. I'm trying to make the I-CUBE-LRWAN AT-master example run on the Nucleo L073rz. As documentation explain i opened SB13 and SB14 and closed SB62 and SB63, i also redirected the...
Hi,I'm using STM32 Lora Discovery kit to run the code generated by cubemx for RTC, While on debug i'm get the RTC values but when run normally then i'm not getting any values except the initialised values for the time.Thanks & Regards,Vijay Rakesh
could you give me any hints what changes are needed to convert IP64Router example from 6LPETH1 (Nucleo-F429ZI + X_NUCLEO-IDS01A4) into an IPv6 router ?
Does anyone use STM32WB55 now? The Reference Manuals is not available on this website.Neither KEIL nor IAR seem to support the chip�?
Hi, I am modifying the sample program End_Node on the kit B-L072Z-LRWAN1.UART2 is configured as a virtual com and works correctly on PA2 and PA3 pins. I'm trying to add a second serial on PA9 and PA10 but I can not receive and transmit anything. I th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.