2025-02-09 8:53 AM
Hi,
I want to report two code generation bugs in Cube MX for Zigbee projects:
I hope you can follow what I mean and fix those bugs. Thanks
2025-02-10 5:29 AM
Hello @vh789,
Thank you for this report.
Can you please mention the version of CubeMX you are using and join the IOC file to analyze ?
Best regards,
Ouadi
2025-02-10 9:46 AM
2025-02-17 4:46 AM
Hi @vh789
Thanks for sharing your IOC file.
I regenerated the source code based on the provided IOC file with CubeIDE v1.17.0 and the result was as expected.
Color Control cluster : the cluster is configured on Endpoint 20, only colorControl_server_1_move_to_color_xy is enabled :
Generated code :
#define SW1_ENDPOINT 20
/* ColorControl server */
struct ZbColorClusterConfig colorServerConfig_1 = {
.callbacks = ColorServerCallbacks_1,
/* Please complete the other attributes according to your application:
* .capabilities //uint8_t (e.g. ZCL_COLOR_CAP_HS)
* .enhanced_supported //bool
*/
/* USER CODE BEGIN Color Server Config (endpoint1) */
/* USER CODE END Color Server Config (endpoint1) */
};
zigbee_app_info.colorControl_server_1 = ZbZclColorServerAlloc(zigbee_app_info.zb, SW1_ENDPOINT, zigbee_app_info.onOff_server_1, NULL, 0, &colorServerConfig_1, NULL);
assert(zigbee_app_info.colorControl_server_1 != NULL);
ZbZclClusterEndpointRegister(zigbee_app_info.colorControl_server_1);
Same for Water content measurement, the code generated is aligned with the configuration, it uses 3 endpoint as expected.
Did you get the same result ? if yes, what is the issue ?
Regards,
Ouadi
2025-02-18 9:06 AM
Hello Ouadi, thanks for trying it.
In my project, I have to place capabilities in the user code below. However, they get removed when regernating the project.
struct ZbColorClusterConfig colorServerConfig_1 = {
.callbacks = ColorServerCallbacks_1,
/* Please complete the other attributes according to your application:
* .capabilities //uint8_t (e.g. ZCL_COLOR_CAP_HS)
* .enhanced_supported //bool
*/
/* USER CODE BEGIN Color Server Config (endpoint1) */
/* USER CODE END Color Server Config (endpoint1) */
};
Regarding the water content sensors, they are configured in endpoints 21-23 (which equals the defines SW2_ENDPOINT-SW4_ENDPOINT. However, the endpoint regstrations use SW1_ENDPOINT.
zigbee_app_info.water_content_server_2 = ZbZclWaterContentMeasServerAlloc(zigbee_app_info.zb, SW1_ENDPOINT, ZCL_CLUSTER_MEAS_HUMIDITY, HUMIDITY_MIN_2, HUMIDITY_MAX_2);
//...
zigbee_app_info.water_content_server_3 = ZbZclWaterContentMeasServerAlloc(zigbee_app_info.zb, SW1_ENDPOINT, ZCL_CLUSTER_MEAS_HUMIDITY, HUMIDITY_MIN_3, HUMIDITY_MAX_3);
//...
zigbee_app_info.water_content_server_4 = ZbZclWaterContentMeasServerAlloc(zigbee_app_info.zb, SW1_ENDPOINT, ZCL_CLUSTER_MEAS_HUMIDITY, HUMIDITY_MIN_4, HUMIDITY_MAX_4);
Thanks
2025-02-19 4:52 AM
Hello @vh789,
You are right, I reported the issue under an internal ticket number 203588.
The issue will be fixed in the upcoming releases.
Thanks and best regards,
Ouadi
2025-02-22 10:44 AM
Hello Ouadi, I have encountered one more problem with CubeMX that I would consider a bug and need halp.
I have a new Computer with new Toolchain install and when I opened my CubeMX project I was asked to migrate the project from STM32Cube_FW_WB_V1.20.0 to STM32Cube_FW_WB_V1.21.0, which I did.
However, now I get erros like the following:
C:/Users/valen/STM32Cube/Repository/STM32Cube_FW_WB_V1.21.0/Middlewares/ST/STM32_WPAN/zigbee/core/src/zigbee_core_wb.c:3704:14: error: 'MSG_M0TOM4_STARTUP_FINDBIND_EP_CB' undeclared (first use in this function); did you mean 'MSG_M0TOM4_STARTUP_FINDBIND_CB'?
3704 | case MSG_M0TOM4_STARTUP_FINDBIND_EP_CB:
C:/Users/valen/STM32Cube/Repository/STM32Cube_FW_WB_V1.21.0/Middlewares/ST/STM32_WPAN/zigbee/core/src/zigbee_core_wb.c:644:20: error: 'MSG_M4TOM0_STARTUP_FINDBIND_EP' undeclared (first use in this function); did you mean 'MSG_M4TOM0_STARTUP_FINDBIND'?
644 | ipcc_req->ID = MSG_M4TOM0_STARTUP_FINDBIND_EP;
To be able to continue working, I reverted my repository and tried to continue with the older Version of the FW package.
CubeMX tried to download it and unpack, which took very long and ended in the white screen.
Therefore, I can no longer use my project and need support on how to solve this.
Thanks
2025-02-23 6:31 AM - edited 2025-02-23 6:32 AM
Hello,
A new version of STM32CubeMX v6.14 will be released very soon with some enhancements.
Regarding your issue, CubeMX will be based on the pack STM32Cube_FW_WB_V1.21.0 to migrate the project with the new dependances as "Middlewares" , if you get some errors, I assume that the pack STM32Cube_FW_WB_V1.21.0 is missing some files and I recommend to redownload it manually from our official website : https://www.st.com/en/embedded-software/stm32cubewb
MSG_M0TOM4_STARTUP_FINDBIND_EP_CB should be declared in the file : /STM32Cube_FW_WB_V1.21.0/Middlewares/ST/STM32_WPAN/zigbee/core/inc/stm32wbxx_core_interface_def.h
Best regards,
Ouadi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.