2021-09-15 4:07 PM
Hey community, it took me some time to track this bug down because I thought I wasn't implementing the sequencer library correctly and was looking at my own code.
Turns out, there is a bug with stm32_seq.c. Every time I ran a task with UTIL_SEQ_SetTask() with a priority over 2, the STM would get a hard fault.
Turns out that setting SEQ_CONF_TASK_NBR and SEQ_CONF_PRIO_NBR, DOES NOTHING because stm32_seq.c is actually using UTIL_SEQ_CONF_TASK_NBR and UTIL_SEQ_CONF_PRIO_NBR. There is a discrepancy between the defines of the two files. This is just am FYI for anyone using the sequencer utility library.
Replacing SEQ_CONF_TASK_NBR with UTIL_SEQ_CONF_TASK_NBR and SEQ_CONF_PRIO_NBR with UTIL_SEQ_CONF_PRIO_NBR in utilities_conf.h will solve this problem.
2021-09-16 12:26 AM
Hello @ECarr.1 ,
You are right, there is an issue here. THanks for pointing this issue at us.
We could fix it as:
1- include utilities_def.h in utilities conf.h
2- define UTIL_SEQ_CONF_TASK_NBR as CFG_SEQ_Task_NBR
3- define SEQ_CONF_PRIO_NBR as CFG_SEQ_Prio_NBR
then in utilities_def.h, you can add more tasks and prio within the enum. Hence, the UTIL_SEQ_CONF_TASK_NBR and SEQ_CONF_PRIO_NBR would be automatically incremented.
Let me know if this would work for you
Sorry for the inconvenience,
best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.