2021-09-16 12:16 AM
Hi,
I'm working with STM32WB5MM, the application is a ble application with freertos.
I have this issue, at boot, on custom board the cpu2 not start every time, so, when this happend APP_BLE_Init() is never called, and because at boot is request to start advertising when I try to start advertising it block and the board is reset by wdt. When it enter in this issue it never unblock. The same firmware could work fine if I try to cut off Vcc and plug in it again, so I can block or unblock the firmware quite quickly by cut off and pugin the power line. If I try to debug in with debugger it unblock, it never block under debug ifI try to put a breakpoint before or after cpu2 initiliazzation so I can't understand what happend, if I try to run code withouth breakpoints it block but I can't understand where it block.
If I try run the same code on demoboard STM32WB5MM diskovery kit it never block if I press reset button, seem impossible to block it by reset button, but it blcok if I plug and unplug JP1, so enabling and disabling Vcc to the system, but in this case after a reset by wdt it start correctly.
So, what should be the issue? Can you give me any suggestion for try to solve this problem?
thank you
Luigi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.