2024-12-02 2:12 AM - edited 2024-12-02 12:36 PM
Issue
Higher ambient temperatures cause communication malfunctions with XSPI memories.
Details
Our design is heavily adopted from STM32H7S78-DK which also has the same issue described below.
The application uses memory-mapped mode for both Flash and RAM as the main operational units. These memories are configured in the bootloader and everything generated using CubeMX. According to the datasheets, all three components (CPU, Flash, and RAM) are specified to operate reliably under the given conditions, and they do function correctly under normal temperatures.
The problem arises when the ambient temperature increases from 25°C to 60°C. These temperatures are within the acceptable operating range for all components, as stated in their specifications. Upon reaching higher temperatures, the memories start to exhibit failures. However, further investigation revealed that the issue is not with the memories themselves. When the memories alone are heated, they continue to operate reliably, even at elevated temperatures.
The issue was traced to the CPU. When the CPU is heated, the failures begin around 55°C. At this point, the CPU starts to malfunction in its communication with the memories. This leads to the CPU entering an undefined state, with fault reports showing inconsistent and varying results.
Lowering the temperature restores normal operation.
Investigations
Specifications
CPU - STM32H7S7L8H6H
XSPI1 - APS256XXN-OBR-BG
XSPI2 - MX25UW6345GXDI00
STM32CubeMX ver 6.13.0
STM32CubeMX package STM32H7RS v 1.1.0
VCC 3.3V
XSPI1 & XSPI2 1.8V
CPUCPLK 600MHz
HCLK 300MHz
XSPI1 & XSPI2 176MHz with no prescaler
ZIP
schematics, layouts, scatter file, mxcube configs & clocks, option bytes
Solved! Go to Solution.
2024-12-03 4:18 AM
Dear @Ondrej Meca ,
Thank you got confirming it . We will release soon a Knowledge Article on the Topic, on How to use this feature in real time application for such High end MCU running from XSPI memories .
Ciao,
STOne-32
2024-12-02 2:13 PM - edited 2024-12-02 2:14 PM
Dear @Ondrej Meca ,
First, Thank you very much for the detailed reporting case which seems very clear .
I give you one hint if you can check it and change your code accordingly :
One hypothesis is that when automatic mode is activated and for each CSI clock cycle , the code may change in run time when temperature is reaching a certain point and if this happens during a transmission or reception the data be corrupt or wrongly decoded by the CPU / System . Please let me know if you need further assistance for your code change .
Hope it helps ,
STOne-32
2024-12-03 3:11 AM
Hi STOne-32,
Thank you for your quick response. After investigating your suggestion, I can confirm that the issue was related to automatic compensation.
I programmed the calculated compensation value from SBS_CCVALR to SBS_CCSWVALR and adjusted XSPI1_COMP_CODESEL and XSPI2_COMP_CODESEL in SBS_CCCSR. After making these changes, the issue was resolved immediately.
However, I have a question: is there any application note that describes this behavior? Should I repeat these steps after every restart, especially if the CPU restarts at higher temperatures (which might result in different compensation values being written at higher temperatures)?
Is this the intended behavior, or did I overlook something?
2024-12-03 4:18 AM
Dear @Ondrej Meca ,
Thank you got confirming it . We will release soon a Knowledge Article on the Topic, on How to use this feature in real time application for such High end MCU running from XSPI memories .
Ciao,
STOne-32
2025-03-10 2:00 AM
Dear @STOne-32 ,
does this mean, that the STM32H7S78-DK Board might also be affected by memory corruption as all demos included in the STM32CUBEH7RS-V1.1.0 are setting up the compensation cell for external XSPI RAM in automatic mode?
See for example:
STM32Cube_FW_H7RS_V1.1.0\Projects\STM32H7S78-DK\Templates\Template_LRUN\Boot\Src\ stm32h7rsxx_hal_msp.c:
/* Configure the compensation cell */
HAL_SBS_ConfigCompensationCell(SBS_IO_XSPI1_CELL, SBS_IO_CELL_CODE, 0U, 0U);
HAL_SBS_ConfigCompensationCell(SBS_IO_XSPI2_CELL, SBS_IO_CELL_CODE, 0U, 0U);
/* Enable compensation cell */
HAL_SBS_EnableCompensationCell(SBS_IO_XSPI1_CELL);
HAL_SBS_EnableCompensationCell(SBS_IO_XSPI2_CELL);
/* wait ready before enabled IO */
while(HAL_SBS_GetCompensationCellReadyStatus(SBS_IO_XSPI1_CELL_READY) != 1U);
while(HAL_SBS_GetCompensationCellReadyStatus(SBS_IO_XSPI2_CELL_READY) != 1U);
/* high speed low voltage config */
HAL_SBS_EnableIOSpeedOptimize(SBS_IO_XSPI1_HSLV);
HAL_SBS_EnableIOSpeedOptimize(SBS_IO_XSPI2_HSLV);
So when the environment temperature changes the compensation cell might be adjusted automatically which could lead to memory corruption when happening while reading from the external memory?
If this is the case how do we have to change the example code to ensure that no memory corruption will occur?
Thank you and best regards
rk_iot
2025-08-14 11:33 PM
@STOne-32 since this topic is over 8 month old is there already a clear article in the knowledgebase who to handle this? We wan in the exact same issue just running a memory test through XSPI and the proposal seems to work. However clear instructions from the manufacturer are always preferred in these cases.
2025-08-14 11:48 PM
Dear @taste ,
Thank you for the follow-up, the Article is under analysis now and will be published soon by September as we wanted to carry more testings and have full corners cases to provide solid workaround.
Can you please let us know your exact XSPI Frequency selected ? and if running with 200MHz , can you let us know the exact code your found (X,Y) for ANSCR = X, APSCR = Y ?
Thanks for your understanding.
Regards,
STOne-32.
2025-08-17 10:57 PM
Dear @STOne-32
We are also waiting for a more detailed solution to this issue as we have build a board based on the STM32H7S78 and need to ensure that the XSPI RAM integration is working perfectly stable.
You said that:
One hypothesis is that when automatic mode is activated and for each CSI clock cycle , the code may change in run time when temperature is reaching a certain point and if this happens during a transmission or reception the data be corrupt or wrongly decoded by the CPU / System . Please let me know if you need further assistance for your code change .
Was this hypothesis confirmed in the meantime and what code changes need to be applied to the examples of the STM32H7S78-DK board to avoid memory corruption when the environment temperature changes?
We are running our board with a XSPI frequency of 200 MHz. We could not find the values for ANSCR and APSCR in the source code or datasheet for the STM32H7S78 can you tell us where to find this values?
If you could provide more details on the proposed solution we would be happy to try your solution on our board and report if this could solve the XSPI RAM instability.
Thank you and best regards
rk_iot
2025-09-22 5:43 AM
Is there any update on when the application note is likely to be available?
If using the manual setting, do you recommend periodically updating it using the values in CCVALR (presumably ensuring that there's no activity on the XSPI buses while doing this)?
2025-09-30 12:55 AM
@Steve Melnikoff wrote:(presumably ensuring that there's no activity on the XSPI buses while doing this)?
+1: how may I ensure there's no activity on XSPIs on a cached ROM-less system with framebuffer on external RAM?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.