2025-05-12 7:13 PM - last edited on 2025-05-13 1:02 AM by Andrew Neil
example code : MRSUBG_WakeupRadio_Tx of STM32Cube_FW_WL3_V1.1.0
board : NUCLEO-WL33CC1
compiler : Keil
running the code, at first message below will shown on Virtual Com,
"STM32WL3 LPAWUR - Transmitter example.
Use PUSH Button 2 to send a frame."
but after pushing Button 2 on board, no message is shown on Virtual Com?!
2025-05-26 8:57 AM
Hello @Gwo
Behavior reproduced and escalated internally for review on the future (Under internal ticket number 210819). For now, you can still use the Version throw the STM32CubeIDE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.