NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Good day,I want to measure the VBAT voltage of a STM32WL31 using its ADC. I setup the ADC channel as follows using the ST HAL driver:ADC_ChannelConfTypeDef ConfigChannel = {0}; ConfigChannel.Channel = ADC_CHANNEL_VBAT; ConfigChannel.Rank = ADC_RANK_1...
I upgrade my project recently to the above firmware (STM32Cube FW_WL V1.5.0) which ended up not working.Lots of errors, I think mostly because of the introduction of the relay node.After a couple of days trying to get this working I started a fresh ...
Dear Team,I have a board contain STM32WBA5MMG and AD5941. We have provided a single RESET for both the chips.The circuit is given below.May Iknow will this cause any issues. RegardsHiyo
When I followed the link https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32_Sniffer_for_BLE_Setup_guide,I successfully make Neclueo-WB55 be sniffer device while STM32WB sniffer displayed in the wireshark startup page,meanswhile I really capture the...
Stm32l010r and s2lp using x cube sub ghz , for custom board just for coding only gpio button status, there are plenty of error, by solving all those 4-5 errors remain and their resolving method is to complete change of middleware files or some code l...
I need support for the design of STM32WL30XX PCB Antenna. Are there reference designs available for the PCB antenna?Specifications:Two layer board Output power 10dBm in the 868MHz band.
Hi everyone,I’m currently working on a project involving LR-FHSS and I’d like to know whether there are STM32-compatible end devices and gateways that already integrate LR-FHSS-capable radio chips.From what I’ve found so far:End Devices (sensor/node)...
I'm designing a custom board that's based on the STM32WL55CCU6 microcontroler. It's very simple and is required to transmit data continuously in vectors of 12 uint8_t elements, using the LoRa protocol configured to the standard values: 915MHz, CR 4/5...
Hello, I am working with the following setup: Board: B-L4S5I-IOT-01AMCU: STM32L4S5VIT6BLE Module: BlueNRG-M0+ (in built in the Kit) I am currently facing an issue related to the BLE MTU (Maximum Transmission Unit) size. By default, the payload length...
Hi, I want to acquire an audio signal from the microphone IMP34DT05 which is connected to the SAI interface of my STM32WB5MM-DK demo board in this way: L/R -> VDD; CLK -> SAI_CK2; DATA -> SAI_D2.The part number I chose is STM32WB5MMGH6TR in STM32Cube...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.