STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

maximizing power save of stm32WL STANDBY_MODE

Hi,I'm trying to move stm32WL to a mode it will consume least power but still be usable for me.I understood this mode is probably STANDBY_MODE with memory retentionI want to do this:1. [Save Stack For Standby] save the stack and any other needed info...

aviad by Associate
  • 686 Views
  • 1 replies
  • 0 kudos

ping pong example is not working

hey i am using the stm32wle5 board , i try to use the ping pong example from the package provided by stm and it was flashed succesfully but when i checked the serial monitor it is showing timeout for both rx and Tx . I have attached the serial monito...

PINGPONG.PNG

Resolved! BLE materials

Good day, I was at a training some time ago: https://content.st.com/stm32wb09-workshop-ame.htmlunfortunately I lost these educational materials. Does ST have them published somewhere on the website? Does ST have materials regarding BLE?

bfijal by Associate
  • 573 Views
  • 1 replies
  • 1 kudos

Resolved! BLE_HeartRateThreadX example file ioc not present

Hello!i'm trying the example BLE_HeartRateThreadX but the ioc file is not present in the directory, is that normal? i'm missing it? also the directory arent arranged like a project maked with cube ideis it possible to have an example that is maked li...

ABasi.2 by Senior
  • 2288 Views
  • 9 replies
  • 2 kudos

Readout protection level 1

Hi team, I am using the STM32WLE5CC microcontroller and I am facing an issue with Readout Protection Level 1. I am utilizing the open bootloader from ST and updating hex files using the STM32Cube Programmer software using USART. Up to this point, eve...

kRaje.1 by Associate II
  • 1100 Views
  • 3 replies
  • 0 kudos

STM32LE5 blocks main thread during lorawan uplink

I have an application consisting on two different tasks:1. Control a DMX bus which requires the MCU to transmit a command to the UART every 22ms2. Send an uplink message via Lora periodically (every 10 seconds for example)I am using the RAK3172 SoC w...

ASL07 by Associate
  • 795 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.